Other Parts Discussed in Thread: BQ25713, , EV2400, BQSTUDIO
Tool/software: Code Composer Studio
h
i am working on a bms system with bq25713 as charger controller. For familiarising the functionalities i have bq25713evm-017. With adaptor input, the charger is able to buck and boost the voltage as per minimum system minimum voltage() i set. but when i working with battery only and disabled adaptor input, controller not able to buck or boost the output voltage. is there any extra setting need to be done on the charger controller in order to works in battery only mode for setting in correct system voltage.
if there is any programming document available for bq25713 controller for setting the functionality other than the datasheet.
thanks,