Hello TI,
We are using BQ24773 for 1 cell charging by using 5V/4A input adapter and 5Ah lithium Ion battery, Load is Raspberry PI
We are facing issues on ACOK, when adapter is connect as per the Charging IC ACOK is provided 3V3, ACOK pin is Pull high as per the reference design by using 10K & 3V3
1. ACOK signal is not stable, when adapter connected we are expecting stable ACOK Output, is it right ...?If yes, how to stable it ..?
2. when load is connected and system is running properly with BQ24773 configuration suddenly system stop after some time charging battery and started discharging, when replace the input adapter it started charging again ..?
3. How to get stable ACOK Output, based on that we configure the system
4. How to identify battery is charging or not, there was any provision across the BQ24773 to identify it ..?
Thank you,
Rahul