This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5401: Need an AC-DC converter

Part Number: TPS5401

Hi, support,
I am looking for a cheaper AC-DC converter and thus I came across TPS5401 of Texas Instruments. 

I need a circuit with a 3.6V output voltage with a 300mA output current from a single-phase AC supply.

The output of TPS5401 is 500mA, but as per the application note SLVA491, the output of the circuit is only 50mA.


The maximum input voltage of TPS5401 is 42V.

Does this mean a 300mA output current is not possible with this chip?.

How can I improve the circuit to get 300mA output current?.