I have a design which implements the TPS5130 and I have a problem where if the power supply behind me has a slow ramping output TPS5130 doesn't start at all. If I turn on the previous power supply (at 13.8 volts) and push the power button on my board later, TPS5130 starts and generates the voltages I need.
So far I checked the reference output at .85 and the internal regulator outputs which are OK even when the controller doesn't start. Any idea why a TPS5130 doesn't give switched dc output when the input voltage is ramping very slowly?