Other Parts Discussed in Thread: BQ25703A
Hi,
I want to charge 1 cell 18650 Lithium battery by BQ25703A EVM. I tested the board as well as downloaded the software following the user's guide and datasheet of the chip. I powered the board up by 5V and I did not connect the load to VSYS. I took JP2,3,4 off and connected a 3.7V 18650 battery and measured roughly 16 mA flowing and 3.6V across it. I left it connected for 2 hours and the current decreased to 0mA. That makes me think that the battery was discharging all the time not charging. In the software, under charge status register, it said not either in fast charge or in pre-charge.
Can you help me how to recognize if it is charging or what I can do (changing which register?) to have the battery charging? I think the board is set to charge the battery as default, is that correct?
Thank you!