Other Parts Discussed in Thread: BQ27Z561, BQ25703A, EV2400
Hello,
I have a design using the BQ25703A charger IC and the BQ27Z561 fuel gauge. I've been able to get BQStudio to communicate with each of them, however I am finding that after I flashed the FW on the fuel gauge to the latest, and this allowed it to be auto-detected, that I can't easily switch between which device I am talking to. They are on the same I2C bus and thought I would not have an issue, but now the application opens automatically into the fuel gauge screen and I can't switch out of it to the BQ25703A screens. Do I need to open the application prior to connecting the EVM? Is there a way to manage two simultaneous instances of BQstudio? I'm trying to set everything up to perform learning cycles and get the fuel gauge calibrated, any help or reference documentation would be great.