Part Number: TPS25942L
Other Parts Discussed in Thread: TPS25944L
Hi
Does the condition of TPS25944L LATCHED include OVP?
Because the second TPS25944L is turned off by OVP, will the second TPS25944L fail to turn on?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
I understand that you are implementing Priority Power Mux operation and not paralleling.
If there is a OVP or OCP event on U27, this efuse (U27) will turn OFF and the output goes to 0V.
This means that OVP of U28 is pulled low which turns the U28 efuse ON. Now, it depends on the PSU2 and Load if an OVP or OCP event also happens on U28 and turns it OFF.
Hi Praveen
U27 FLT and PGOOD are both MOSFET grounded, change to FLT to operate normally,
1. When U27 OVP, U28 OVP is connected to U27 PGOOD, the output is no voltage (PGOOD still has 1V voltage)
2. When U27 OVP, U28 OVP is connected to U27 FLT, the output is U28 output
3.U27 =>MAIN PSU / U28=> BACKUP PSU
If U28 OVP is changed to U27 FLT, when the voltage of U27 is less than the voltage of U28, the output will be fixed by U28 and cannot be switched back to the main power supply of U27, unless U28 fails or the voltage is less than U27
Hi Gareth,
Yes, you are right. If it is an OVP condition on U27 and not a UVLO condition, the PGOOD will still be high and U27 will turn OFF itself as well as U28.
In this case the FLT/ will help in turning ON U28 when U27 has OVP.
Hi Praveen
Thank you very much
1.PG1 is the open drain pull low, where does 1v come from?
2.Because when U28 is not powered on, U27 has OVP. At this time, PG1 is 0v ......
2. If U28 OVP is changed to U27 FLT, when the voltage of U27 is less than the voltage of U28, the output will be fixed by U28 and cannot be switched back to the main power supply of U27, unless U28 fails or the voltage is less than U27
Hi Gareth,
Thanks for sharing the waveforms.
Hi Praveen
Sorry I update the current schematic as EVM
schematic is set as follows
removed (R19, R26, D5, D9, C4, C10)
J1 2-3 connect together
R8 short
Waveform as follows
Hi Gareth,
Looks like you have applied over voltage at the input of Channel 1 and the device has turned OFF its output. This is why the CH1 has turned OFF.
Are VOUT1 and VOUT2 tied together ? What is the voltage applied on Vin2 ?
Hi Gareth,
If Vin1 goes above OVP and turns OFF, the PG1 should go low and as it is tied to OVP2 the channel 2 TPS25942 should turn ON and power the load.
I don't see any reason why the PG2 should go low.
Hope VIN1 and VIN2 are independent power supplies.
Hi Praveen,
We have independent source for Vin 1 and Vin 2. In our test today on EVM,
1. When we don't tied Vout1 and Vout2 together, the result looks good.
2. When we tied Vout1 and Vout2 together (J1 is in 2+3, PGTH tied to Vin), we see 1V on PGOOD1 so there's no output on Vout...
3. If we change J1 sett to 1+2 (PGTH tied to Vout), Vout is swithing in 0V and 12V.
Please help to check it at your side and see how do we have to setup our environment.
Regards,
Gareth
Hi Gareth,
The root cause of the problem is that the PGOOD signal is not pulled low by the controller when there is an OVP event.
The PGOOD continues to be high and reflect the Pullup voltage (Vout1). So, initially when there is an OVP event, the output keeps discharging anf the PGOOD also follows output as PGOOD is pulled upto Vout. Once the PGOOD-1/OVP-2 reaches less than ~1V, the Channel-2 turns ON and the OUTPUT starts to ramp up. When Vout ramps up, the PGOOD-1 and OVP-2 also ramp up there by turning OFF channel-2. This continues in a cycling process and the VOUT oscillates.
The Priority Muxing configuration mentioned in datasheet is not recommended for input OVP conditions.
Hi Praveen
Thanks for your assistance
When using one channel , when IC OVP PGOOD is low
Why another pin FLT can be pulled LOW when OVP , But when ch1 returns to normal, ch2 cannot switch to ch1
ch1 voltage must be greater than ch2 voltage to switch back to ch1
Hi Gareth,
When the primary power supply is present and within limits the primary channel should supply power irrespective of whether it is higher or lower than the secondary power supply. Please refer to waveform captures from datasheet below.
Please verify the connections on your board and try replacing the IC with new IC and re test
Hi Praveen
Thank you for your support
A-The connection method of waveform captures (Figure 80~83) is PG1 to OVP2 in the datasheet
But when it is changed to FLT1 to connect to OVP2 ,When the voltage of U27 is less than the voltage of U28, the output will be fixed by U28 and cannot be switched back to the main power supply of U27, unless U28 fails or the voltage is less than U27
B- When PG1 is connected to DMODE2, it takes a very long time (300ms) for VOUT to switch to PSU2 after PSU1 is turned off.
Will it not be (400uS) when changing to FLT1 and DMODE2? But does DATASHEET indicate the need to connect PG1 to DMODE2?
Hi Gareth,
In Condition 1 where FLT1 is connected to OVP2,
When Vout is greater than Vin1, the FLT/ is asserted due to reverse voltage and this will turn ON Ch-2. Similarly, CH-2 will be OFF only when it sees reverse voltage that is Vout > Vin2.
In Condition 2 when PG1 is connected to DMODE2 the transition should be very fast as shown below. The below waveform is captured with Cout = 150uF and Rload = 4 ohms. What is your Cout and Rload ? Can you restest with Cout = 150uF and Rload = 4 ohms ?