This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61253AEVM-803: noise is emitted from the circuit at 5 ohm load.

Part Number: TPS61253AEVM-803
Other Parts Discussed in Thread: TPS61253A, TPS61022

noise is emitted from the circuit at 5 ohm load. LIPO battery is being used with a 3.7/3.8 Vin. The circuit seems to not be able to handle that low of a load. When the load is increased like to 200 ohms, the circuit seems to work fine. This issue happens in both PWM and PFM mode. If someone could give me some insight on why this is happening I would appreciate it.