This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5164-Q1: PGOOD Operation

Part Number: LM5164-Q1
Other Parts Discussed in Thread: LM5164

Hi Team,

I had a question about the PGOOD pin operation of LM5164.

Following is the requirement:-

If the DC-DC output voltage is greater than 110% of rated output or less than 90% of rated output, then the ECU shall be notified.

Can this requirement be fulfilled via PGOOD pin?

The block diagram shows that the PGOOD pin comparator compares its value to 90% of FB value. What about 110%?

Thanks,

Rohan Patwardhan