Other Parts Discussed in Thread: PMP10215, , PMP40281, UCC256402
Hi, TI expert,
Currently need to make a two-tube forward design with 300~1000V input Voltage, 24V output Voltage and 200W output Power.
Suppose LM5021 is the suitable device for this design, taken PMP10215 as a reference.
Q1: Do you have a better device to recommend?
Q2: Is there any documents to guide the design of transformer and Inductance parameter within the Two-tube Forward Circuit?
Best Regards,
Jayce Luo