This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2992: ON/OFF Function

Part Number: LP2992

Hi,

The following is written on the datasheet of 7.4.2.

"If this feature is not to be used, the ON/OFF input must be tied to VIN to keep the regulator output on at all times. "

"To prevent mis-operation, the turnon (and turnoff) voltage signals applied to the ON/OFF input must have a slew rate which is ≥ 40 mV/µs. "

Does it mean that VIN slew rate must be upper 40mV/us when ON/OFF pin is tied to VIN?

Best Regards,

Kuramochi

  • HI Kuramochi-san,

    The slew rate statement on the ON/OFF pin is made with respect to driving it externally. If the ON/OFF pin is tied to VIN, this limitation should not apply. 

    I hope this answers your question.