This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: IC doesn't sleep when LCD is active

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ76930, BQSTUDIO, BQ20Z655-R1, BQ78350

Hi,

I have designed 10 series BMS with BQ78350-R1 and Bq76930. I added LCD on my pcb.

When data flash parameters are default on BQ78350-R1, LCD doesnt work and device can get into sleep mode.

But when I enable LCD, LCD shows the SOC but the device doesnt get into Sleep mode.

I would like to see segments on LCD even its in sleep mode. What should I do?

DA Configuration > Sleep bit is set.

LED Configuration > LCDEN bit is set.