This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A24: About individual limit of R1 and R2

Guru 21045 points
Part Number: TPS7A24


Hi Team,

 

We found “R1 + R2 ≤ VOUT / (IFB × 100)” in datasheet.

However, we would like to know the individual limit of R1 and R2 because use the following condition.

Could you please let us know if you have any concern for the following resistor values?

 

[Our conditions]

R1 is 1Mohm

R2 is 120kohm

Target VOUT is around 11.5V

*We would like to use large resistor because decrease the consumption current.

 

Regards,

Hide

  • Hi Hide,

    The nominal IFB current is 10nA so with R1 = 1Mohm and R2 = 120kOhm we have

    11.5V/(100*10nA)= 11.5Mohm

    Since your solution has R1+R2=1.12MOhm  is meeting the limitation highlight in equation 3:

    The reason for this constraint on the feedback resistors is simply that we like to see the current leakage through R1+R2 be strong enough to swamp out any leakage into the FB pin as this could impact output regulation accuracy. 

    I hope this answers your question. 

  • Hi JCHK-san,

    Thank you for your prompt reply.

    I greatly appreciate your cooperation.

    Regards,

    Hide