Other Parts Discussed in Thread: TLV751, TLV755P
I can not find this value on the datasheet. In my design, TLV711 is msut able to drive more than 50uF.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I can't find any details on a maximum output capacitor. In general, for stability more than 50uF should be OK, but my key concerns would be inrush into the load. This could cause a non-monotonic rise and possibly some drop on the input rail.
We do have the TLV751 which has a recommended maximum output capacitor of 220uF. This might be a better choice if you need a very large output capacitance.
I hope this answers your question.
The LDO should be able to output 1.8V and 2.9V(2.85V). For TLV751, the P/N seems to be TLV751180290(TLV751180285). But I can not find them anywhere.
This is a space senstive project. Dual output LDO with fixed version is best choice.
Hi,
At the moment we only have the 1.8/2.8V fixed released https://www.ti.com/store/ti/en/p/product/?p=TLV751180280PDSQR
Can you share the application needing 1.8 and 2.85V?
Thanks,
Based on that the TLV711 is probably your best choice. Do you need help in ordering an EVM to see how it behaves when you have more the 50uF at the output?