Other Parts Discussed in Thread: TIDA-01560, , UCC28701, UCC28722
Hi,
I'm designing a 3-phase PSU and the TIDA-01560 ref design meets my requirements. I'd like to alter the AC input adding a 3phase full-wave bridge rectifier to this ref design, and then replace the Mosfet with a higher voltage model, and have the following questions:-
1. Do you have an EMC filter design suitable for 3phase that you can recommend.
2. For 230Vac phase-to-neutral voltage with full-wave rectification, the DC voltage will be ~566V. If the 3-ph phase-to-neutral voltages exceed 285Vac then the DC voltage will exceed the 700V limit for the HV pin. Can I protect the HV pin for this situation?
3. Is there anything else I need to consider or alter for this wide input range design?
Thanks
Tony