Other Parts Discussed in Thread: AM4376,
- We are using a TPS65218D0 to power a AM4376 CPU
- In the TPS manual there is a mention that the AC_DET has to go to IN_BIAS(which is around 5V) if not used
- i. But for Bootup is says AC_DET must be Grounded
Please clarify.
We also will have no power button – the power up will be done by connecting a cable to a connector which will then power some DCDC converter and then IN_BIAS and all other inputs of the PMIC.
- Do you have a reference on the power consumption of the PIMC from the Coin Cell – we are trying to estimate the life of a Coin cell battery in our system or if 2 batteries are needed or a charging circuit + rechargeable battery
- RTC_KALDO_EN Pin. Section 6.4.3.5 Internal RTC LDO of technical reference says "If your application uses the RTC functionality and requires RTC-only mode, the internal LDO is required to enable proper wakeup signaling from the RTC domain.
The proper wakeup signaling requires the following connections:
- RTC_KALDO_ENn is grounded
- CAP_VDD_RTC is connected to 1uF decoupling capacitor to ground
- RTC_PWRONRSTn is connected to 1.8V RTC power on reset
- PMIC_POWER_EN is connected to power input of PMIC
- RTC_WAKEUP (EXT_WAKEUP0) is connected to a wakeup source"
Our design and the General Purpose reference designs have RTC_KALDO_ENn pulled to VDDS_RTC.
Please comment – which one is the right connections