This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610EVM: Inquiry about BQ24610EVM setting

Part Number: BQ24610EVM


I am setting the BQ24610EVM as a 1Cell charging method.

I changed the EVM's R25 to 100k and set the Vbat to 4.2V.

However, STAT1, 2 has no response.

External conditions are:

 - Vin : 12V

 - Bat : Li-ion 1Cell 3.7V, 14Ah 

 - Protection Bat

  : OCV : 4.35V

  : OCA : 8.0A

 - TS no Connection

Do you ever need to change other settings?