Other Parts Discussed in Thread: TVS1800
We are using TPS2121 to switch over from 9V mains to battery boosted voltage 9V. We are using TI Samples for our prototype board.
The SS capacitor section of our board randomly burned today. The load was not connected. TPS2121 had only second source (IN2) from the battery boosted regulator output. 43K & 5.1K are the protection resistors used. We are not sure if the TPS2121 burned of if it was the SS capacitor. The section of TPS2121 with SS pin is damaged and the SS capacitor area seems to have popped and the traces are damaged.
We have a 12V version of the same PCB design running without issues though. It has different switch over and OV resistors. Other TPS2121 components remain the same.
Thanks in advance.