Is there a minimum size for the feedback resistors? Datasheet section 7.3.4 recommends the range of 100KΩ to 1MΩ and warns against larger values, but does not mention smaller values. I ask because I need to handle some reverse current from a diode and I would typically do this with a resistor from the anode to ground. However, since this resistor will be in parallel with the feedback resistors, perhaps I could simply use smaller resistors there and allow them to handle the reverse current. My reverse-current-handling resistor is 1KΩ, so the feedback resistors would be in the range of 250Ω - 750Ω. Do I risk damage to the FB pin with such small resistors?