Hi,
I am looking for an LDO or regulator IC that work with 2.5 to 6V input.
My main supply is 9-28V DC - so using LM1085 to convert that down to 6V, this is going to a battery charger IC having power path.
Output side of the battery charger will then be 6V if running on external supply or 2.5V to 3.6V when running on battery, i.e range is 2.5 to 6V.
LDO output I need 4V , 2A.
Do you have an LDO option that can work for this range?
I found LP3856 /LP3876 but i need to confirm this is still active and I consider this for new designs? (I saw these ICs are 'No Longer Manufactured' in Farnell website)
If you can suggest a better option also would be great.
Regards,
Sarath