In the datasheet for TPS92682-Q1, section 7.5.3 Response Frame there are three types of response frames
1. Read Response Frame: This frame is sent out by the TPS92682-Q1 following a read command
2. Write Response Frame: This frame is sent out following a write command if the previously received frame was a write command and no SPI Error occurred during that frame
3. Write Error/POR Frame: This frame is sent out by the TPS92682-Q1 internal digital block during the first SPI transfer following power-on reset, or following a write command with a SPI Error
My inquiry is, what would be the response frame format in case a write frame was sent to the TPS92682-Q1 following a read frame?