This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM34936: Inductor and R5 is hot

Part Number: LM34936


Hi

I have LM34936 and the inductor and R5,D1 is getting pretty warm, temp close to 60C, can you explain if this is normal or do I have to increase the pad under these components. 

Is this normal or not

The input voltage 24V 

Input current 1.5A

Output voltage 12V

Output current 4A

Thank you