I need some advice on how and when setting the initial remaining charge capacity and how it is updated along the life of the battery. NiMH battery pack, 12V nominal. The fuel gauge is on board, not in the battery pack. FWIW the pack will be in a floating configuration, as power backup in case of mains shortage. Thus, most if its useful life it will stay fully charged.
1- My first basic question relates to how to set the initial charge state of the battery pack in the fuel gauge. As the FG is not in the pack, when I plug a pack I want to be able to set the initial remaining charge capacity (even if an estimated one) of the pack as it may be partially charged. I learned when I reset the FG it uses the current voltage of the pack and it uses the data in the DOD table to set this remaining capacity. From that on, it integrates the current, which is OK.
So my first question is if this is the right approach.
Is there a better or more correct one?
Does it use the learned capacity (which must degrade with battery aging) or the nominal capacity?
2- My second basic question relates to long term remaining capacity. The pack will not discharged to its minimum as the system requires a minimum voltage to work. So we are using only around 60% of the full pack capacity (when new). I need to give the system an estimation of remaining capacity so my 100% will be the pack fully charged, obviously and my 0% will be when the pack reaches 40% (give or take) of its full capacity, when the voltages reaches the minimum my system allows.
Would you have any hint or advice on how to determine the new 100% an 0% along the time? Will the fuel gauge adjust to the pack's aging?
Thanks in advance.