Other Parts Discussed in Thread: LMR14030, LM76002-Q1, LM76003-Q1, , LM76002
I have read several posts here about the Css limitation in the WSON package. Please tell me if this summary is correct:
1 - The issue is only present when EN is controlled externally and the part may be disabled when VIN is present.
2 - The issue is due to the inability of the WSON to completely discharge the Css capacitor, leading to a shortened soft start when the part is next enabled.
Can you give me more details about the issue when a larger capacitor is used? My application needs a very long soft start - as long as 250ms, requiring a 1uF capacitor. Is the issue that the capacitor will take longer to discharge? I can keep the part disabled for a fairly long time, will the Css eventually discharge? Or, if it will never completely discharge, will it eventually drop to some lower voltage? I may be ok with a shorter soft start time.
There is no mention of a limitation for the HSOIC package, but can it handle a Css as large as 1uF? Or is that too large even for this package?
Would it be safe to use an external resistor to help discharge the capacitor? Or a FET to discharge it when the part is disabled?
On a related topic - rather than connect a capacitor to SS, I may want to drive SS externally (with an analog voltage) to control the voltage output. If I do this I may also be able to implement the longer soft start this way, by externally applying 0V and ramping up the voltage. Would this be a safe thing to do? I assume that the voltage on the FB pin would track the SS pin. Will the part indeed work like this?