This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62133: on the same 12V power supply with a DRV8870?

Part Number: TPS62133
Other Parts Discussed in Thread: DRV8870,

On our PCB we plan to use the TPS61233 to generate a stable 5V (1A load) and motor driver DRV8870 (max. 2A load) sharing the same 12V input. Is there a risk that load changes on the DRV8870 lead to noise on the 5V output?