Other Parts Discussed in Thread: TPS2540
I have a design that used the TPS2540. Now due to availability I ordered a batch of PCBs with the TPS2543 which was supposed to be pin compatible.
In my design I need only one current limit. So I hardwired the ILIMSEL signal to GND and hooked up the limit-setting resitor to ILIM0.
In my design I need only one configuration: CDP / BC1.2. So I hardwired the CTL signals to 111 .
So when testing the old boards, I hook up a tablet and it can communicate with the host, in this case an FT312D chip. And the tablet starts charging at 1.45A. Good.
But the TPS2543 boards just consume 0.013A total (the FTDI chip) and no communication happens. Is this expected behaviour for the TPS2543?