This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC34063A: mc34063a or any other low cost part : 12V to 12.6V boost with current limit for 1Amps

Genius 3300 points
Part Number: MC34063A
Other Parts Discussed in Thread: TPS55340, LM3478

Input is 12V, output I need is 12.6V with 1Amps current limit.
Output connected: Lithium battery 8.1V to 12.6V range and a resistive load in parallel.

Since battery is also connected at the output, so current limit is required. Otherwise battery drains huge current, if limit is not there

Is it possible by mc34063a ?