This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS53355: TPS53355 junction temperature

Part Number: TPS53355

Tool/software: WEBENCH® Design Tools

Hi team

what is TPS53355 junction temperature simulation condition? thanks

  1. Airflow?
  2. PCB layout?
  3. PCB copper?
  4. Or other conditions

Jimmy

  • Hi Jimmy,

    The thermal information table on page 6 uses the JEDEC standard board. The application report linked below the table provides more details.

    The SOA curves on page 14 in figures 32 and 33 would be measured using the EVM.

    Anthony

  • Hi Anthony,

    Thanks for your feedback.

    I use WEBENCH to run junction temperature in different ambient temperature simulations for customers.

    And and the customers want to know what conditions are considered in the simulation results of WEBENCH, thanks.

    1. Airflow?
    2. PCB layout?
    3. PCB copper?
    4. Or other conditions

    Jimmy

  • Hi Jimmy,

    The junction temperature calculation in WEBENCH is a relatively simple calculation using a Theta JA of 27.2 °C/W which is actually quite pessimistic. Lower Theta JA can be expected in a real board design. For example, in the default design the TPS53355 has a power dissipation of 1.4W and 30°C ambient temperature. 30°C + 1.4W*27.2°C/W = 68.1°C.

    This number is from the JEDEC standard simulation which does not include Airflow with the JEDEC standard layout which is a 4 layer board with a relatively small amount of copper. In a real application, you can expect much better performance than this. For example, if I up the design to 30 A to match the thermal image in the TPS53355 EVM user's guide, WEBENCH estimates a junction temperature of 128.3 °C while the measurement in the user's guide shows 88.6 °C. Assuming the power dissipation in WEBENCH matches the EVM exactly, this means the EVM Theta JA is around (88.6°C-25°C)/3.8W = ~17°C/W.

    More details on the JEDEC standard can be found in http://www.ti.com/lit/pdf/SPRA953