HI Team,
I haven't find any error data on the die temperature measurement.
Could you pls help?
BR,
Ted Zhang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Team,
I haven't find any error data on the die temperature measurement.
Could you pls help?
BR,
Ted Zhang
Hi Ted,
The temperature measurement accuracy is dependent on multiple factors:
So it depends on the battery monitor and the thermistor, so these must be analyzed together. The pullup resistor value range is covered in the datasheet. The ADC voltage was tested over temperature and the max sigma of the reported voltage and the actual forced voltage was 1.57mV across 25C to 85C. The LDO voltage does vary slightly across temperature (this can be measured on the CAP1 pin).
Best regards,
Matt