This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195L: doesn't complete the battery charge cycle

Part Number: BQ24195L

Dear All,

I'm using the BQ24195L with a 6000mAh Li-Po battery 3.7V.

As indicated in the technical data I've connected a led and a pull up resistor on the STAT port. The port always remains low and it seems the charge cycle doesn't terminate. Why?

The configuration that I'm using are:

 REG00: 0x35

 REG01: 0x1B

 REG02: 0x60

 REG03: 0x11

 REG04: 0xA2

 REG05: 0x8A

REG06: 0x03

REG07: 0x4B

Thanks in advance,

Alan