This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: External control of dvdt pin?

Part Number: TPS1663

Is it possible (and safe) to implement some sort of external control using the dvdt pin?  Sort of like a tracking functionality on a voltage regulator.  I have an application that may want to have dynamic control over the slew rate, or possibly make the slew rate go backwards, to slowly decrease the output voltage (I do understand the power dissipation issues with that).

If anything similar could be done with the ILIM pin, that could be an option for me as well.  Or perhaps some other method I am not thinking of.