Hi,
I've been working with LM46002PWP and have an issue with the output voltage. My input range is 9-36V, the output should be 5V. The current drawn by my load is between 330mA and 600mA. The switching frequency is 400kHz (RT = 100k).
Everything seems to work fine, but after some time, especially after several reboots, the output voltage fails to reach 5V and stays at around 1.7V. When this happens, the input voltage of the output inductor (at the SW pin) is constant, the PWM ceases to work. As you can see below, in the first circle there doesn't seem to be any overvoltage when turning it off, the second circle marks the instant when I turned the board back on. We see something happening but the output voltage doesn't rise. The third circle is after a few seconds, and symbolizes the time when output is stuck at 1.7V, with no PWM observable on SW pin.
I randomly found out that removing the RT resistor helped the chip get back to work after having been locked, since I could observe the PWM working and the expected 5V output, but not for long (after 3-4 reboots the issue's back), I'd think that the LM46002 did not fail completely because the previous action/observation was repeatable.
Here is my schematic. I've never encountered the issue on the 3V3 output.
I thought the chip was having an Hiccup condition, so I added a 45nF cap to the SS pin in order to give some more time to the output capacitor to charge. The test is currently ongoing (I replaced the defficient chip with a new one), and so far so good, but I still expect the power supply to fail at some point because I compared my design with the LM46002PWPEVM's. Every voltage level/wave forms are similar except for one, that is the voltage seen on the RT pin. I removed the RT resistance in both board to have less interference from the rest of the circuits. Thus the pin was left open in both boards and the switching frequency internally set to 500kHz.
Here is what the RT pin voltage looks like on the EVM, we observe a rather nice wave form and a voltage of 2.6V
In comparison, the voltage on the RT pin in my design (with supposedly nothing but the trace length between the resistor pad and the pin) is only rising up to 1V. When turning the board off, it seems that the RT pin wants its voltage to rise back up to 2.6V (like the EVM's) which causes a spike that doesn't appear on the EVM. The voltages is also decreasing to 0V far quicker than the EVM's (see below).
What voltage should I expect on the RT pin ?
Is there an explanation as for why the chip keeps working when replacing RT resistor ?
What would causes the chip to stay stuck at such a voltage ?
I've made plenty of tests and measures. Please ask if you want more information.
Still, the main issue is that the power supply ceases to provides the wanted 5V output after rebooting several times.
Thanks in advance. Best regards
Mickael.