Part Number: TPS61256C
Hi please refer to following PCB design
But the output is about 2.5V..
what is the problem??
Should I need to connect A1,A2 and B1,B2?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS61256C
Hi please refer to following PCB design
But the output is about 2.5V..
what is the problem??
Should I need to connect A1,A2 and B1,B2?
Thanks.
Thanks for your reply
My question is that should I connect both A1,A2 which is Vin and both B1, B2 which is sw?
or can I just use one of them like my picture?(just use A1 and B1)
can you explain with the chip design why there are 2 pins for Vin(A1,A2) and SW(B1,B2)
Thanks
You have to connect both A1, A2 to Vin, B1, B2 to SW.
One pin cannot flow so much current.
It's not suggested to use bread board to test the IC.