Hi Good Day!
I'm working on a 3.3V Handheld system with estimated max possible current consumption of 1.2A. We'll be using a 3.7V 2200mAh Li-Ion battery. We need a solution to charge the battery using a 12V supply from a charging system. To extend the Battery life, While charging we would like to draw current from the 12V supply for the handheld system's load.
So far this is the solution that i thought of:
with 12V input to bq24075 (with the battery connected as specified at specs.). connect bq24075's output to TPS63001 to have a regulated 3.3V output capable up to 1.5A.
Please confirm if this is an efficient solution that my satisfy the above requirements. So far As checked, this is quite an expensive solution. Can you please suggest a cheaper and efficient solution.
Thanks,
John