This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Look for the solution to replace ADF4372

Other Parts Discussed in Thread: LMX2820, LMX2595, LMX2594

Hello E2E,

do we have any solution to replace ADF4372?

https://www.analog.com/media/en/technical-documentation/data-sheets/adf4372.pdf

BR,

Jason

  • Hi Jason,

    We have a few potential solutions:

    • LMX2820 (best match) - Three outputs (one of these can be SYSREF), VCO range 5.6GHz to 11.2GHz, doubler available up to 22.4GHz, in preview now.
    • LMX2595 - Two outputs (one of these can be SYSREF), VCO range 7.5GHz to 15GHz, doubler available up to 22GHz, available today
    • LMX2594 - Two outputs (one of these can be SYSREF), VCO range 7.5GHz to 15GHz, available today

    Regards,