Other Parts Discussed in Thread: LM5060-Q1, LM74800-Q1
Hello,
I am designing a 48V/500W 3-phase motor control system with an external driver for automotive application.
I would like to control the rising voltage on every phase with an LM74700-Q1. The voltage rise is expected to reach 60V and I am using an high power TVS per phase to keep it lower than 55V.
The maximum motor speed is 5000rpm, that is nearly 84Hz on the single phase.
My question is, with the described specifics, what could be the maximum turn-on time for this component if it is supplied from the 48V phase output? Is it better to connect the EN pin to the 48V supply and the Anode to the phase output? Will it reduce the turn-on time?
Is there a more suitable component for this application?
You can find attached the schematic.
Thanks in advance,
Dario Moscardi