This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703AEVM-732: Battery health register

Part Number: BQ25703AEVM-732
Other Parts Discussed in Thread: BQ25703A, EV2400

Hi,

I want to charge 2 Lithium 18650 batteries with BQ25703A EVM and EV2400. I can set charge current limit, charge voltage limit and read charge status. I want to see the battery health while charging. Are there any register that shows health battery?

Besides, while charging 2 batteries in series, if I chose to charge one battery which remained 27% and the other one had 85%, the charge controller stopped charging when the 85% one is fully charged. But I want both battery fully charged. Can you suggest any solutions for this situation?

Thank you