This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51050B: Charging current for small capacity LiPo battery (200mA ~ 300mA)

Part Number: BQ51050B

Dear Sir/Madam,

My customer considers using BQ51050B because it has Qi receiver and charger function.

But I am concerned about charging current.

The minimum charging current is 500mA in datasheet, the battery in product will be 200mA or 300mA LiPo, the customer wants to set the charging current to 0.9C. Is there any way to set charging current to under 200mA or 300mA?

Or could you recommend another part which has Qi receiver and charger function and can set charging current to under 200mA or 300mA?

Thanks,
YY.