This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43060: TPS43060 not working when load is applied

Part Number: TPS43060
Other Parts Discussed in Thread: CSD18534Q5A

Hello

I have design a board wich implies also a boost power stage, that raises from 24Vdc to 42Vdc. I first generated the schematic with Webench tool and after I build up my schematic following the same schematic. The changes that I have done are:

- Inductor from 4.7uH to 5.6uH

- Feedback resistors

- Css to 3,3nF (in the schematics is placed a 100nF but I changed it to be much more compatible with webench).

Enable is drived by a FPGA with a 3.3V signal. Power good is drived to the FPGA for checking status.

What I see is that without load the regulator works. When I attach a load, also small (ie 540 Ohm), the regulator stops to work correctly and the voltage drops down. 

What I checked is that the frequency, during the small periods when the transistors are drived, seems to be right to about 1 MHz like the design.

What could be the issue?