Other Parts Discussed in Thread: UCC27524A
I am not trained in electronics and require assistance in acquiring the correct high-side gate driver for an H-Bridge module which I'm using to switch polarities in electromagnets (by reversing currents of the order of 50A in the DC circuit from a 12V battery).
The module is a Vincotech FZ074PA75SM-L625F08 using IGBTs rated for 75A; Collector-Emitter Saturation Voltage 15V, Gate-Emitter Threshold Voltage 4V.
Someone at the AAC forum suggested using your UCC 23513 isolated gate driver, and I'm wondering if that is appropriate for this application; or whether another component or type of component would be better, such as a half-bridge driver. The further problem in this situation is the need for a bootstrapping circuit.