Hello
My application has 24V input and 3V output with 2.4A maximum current capacity.
I plan to use LM61440 or LM61440-Q1, and will implement external sync function from a FPGA.
My question is:
Which is the proper way to handle BIAS input of LM61440?
My Vin is larger than 16V and highest power rail on board is 3V. Seems no suitable power for BIAS input.
If I could use 5K ohm & 19K ohm resistors as a voltage divider to give a 5V input to BIAS pin?
Thanks