This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Additional capacitance on output of TPS82671

Other Parts Discussed in Thread: TPS82671, TPS82671EVM-646

Team-

We have the following query regarding the TPS82671 and it's tolerance of additional output capacitance:

--------

There are minimum capacitance requirements at the load that I can not control.

Does the TPS82671 have maximum output capacitance constraints? The spec states a maximum of 7uF of external capacitance under PWM mode.

Is this a firm requirement? What if I have a POSCAP on the output, or the caps are isolated with a ferrite bead with DCR = 10m for instance?

--------

Are there any tricks (beads, etc...) that we can use to allow additional capacitance to be added to the output of the TPS82671 w/o making it unstable?

Best regards, S. Dunbar, AFA Colorado