Hi,
- At power up, the LEDs do not always come on. Any one of the 5 chips may fail. However the data still passes through the failed device so we see data coming out of the SOUT pin. So, it we have 2 chips daisy-chained, the first device can fail but the second device can still power up correctly.
- When a chip has failed, we cannot recover it except by power cycling the devices.
- The failure does seem to depend on the power supply voltage but we cannot find a voltage which is consistently reliable.
- When the system powers up correctly, it appears to work correctly thereafter. We have only tested this in a diagnostic mode however which may not exercise all the register settings.
- We are running the GSCLK at 32MHz which is close to the spec limit of 33MHz
- The GSCLK is running asynchronously from a Xtal oscillator so has no relationship to SIN, SCLK and LAT (see attached picture).
- The LED outputs are connected to 16 RGB LEDs to a positive power supply so all 48 outputs are used.
1.Can you check with your design team please that it is OK to run GSCLK asynchronously, or not?
2.Are there any other possible reasons that the device may latch up in a state with all the LEDs off?