Hi
I have project use the BQ25713 to charger 3S battery.
I set the REG0x03/02() to 0x1000H (4096 mA), but charge current can't up to the 4096mA.
I read the battery gas gauge IC current register is show the charger current only 2592mA.
How to set the charger current up to 4096mA ?
Bellow is all register set value.
ChargeCurrent 0x1000 //REG0x03/02
MaxChargeVoltage 0x3138 //REG0x05/04
ChargeOption1 0x0002 //REG0x30
ChargeOption2 0x02B7 //REG0x32
ChargeOption3 0x0030 //REG0x34
ProchotOption0 0x4A61 //REG0x36
ProchotOption1 0x81A0 //REG0x38
ADCOption 0x2000 //REG0x3A
ChargerStatus 0x0000 //REG0x20
ProchotStatus 0x0000 //REG0x22
InputVoltage 0x1C00 //REG0x0B/0A
MinSystemVoltage 0x2400 //REG0x0D/0C
IIN_HOST 0x6FFF //REG0x0F/0E()