Hi there,
I was wondering if it is feasible to use the inductor current instead of the transistor current as a current feedback for the ucc28070?
Thanks,
George
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
I was wondering if it is feasible to use the inductor current instead of the transistor current as a current feedback for the ucc28070?
Thanks,
George
HI, George
UCC28070 have to sense the transistor current because of Advanced Current Synthesizer Current Sensing.
UCC28070 sense the transistor current and transfer to average current of inductor internally, so it is not working if you sense inductor current instead.
BR,
Yunsheng