This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33630: output capacitor howling

Part Number: LMR33630
Other Parts Discussed in Thread: LMR36015,

Hi team,

below is customer schematic, they found the output capacitor will howling when connect load.

customer application as below:

1. input 12V, output 4V/1Amax , usually output current is 300mA, fsw=400kHz

2. inductor L0203 Irms =3.5A, Isat =6A.

4. output capatior 22uF rating voltage is 10V.

3. change R0250 and R0251 to 33K and 11k, still howling.

I also attached SW waveform and output ripple waveform and PCB layout, could you help give some suggestions? thanks

LMR33630 waveform.zip