Could you please help me and share the suitable buck converter part number to consider in our design.
Vinput = 2.4 to 5.5V
Voutput = 0.495 to 0.6550 V (adjustable)
Maximum current output current rating = 3A or higher
Thanks and Regards,
Arumugam.P
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Arumugam,
Can you have a look at the TPS62864 ? It has an I2C adjustable output voltage from 0.4V up to 1.675V in 5mV voltage steps.
QFN spin of this device will soon be available in preview.
Are you willing to consider I2C for your design or feedback with resistive feedback to set the output voltage is preferred?
Let me know if you have other questions.
Thanks a lot!
Regards,
Dorian
Hi Dorian,
Thanks for your support.
I would like to go with Non-BGA LDO due to varies reason.
So i have been consider to use TPS62823DLCR with external I2C dac to control the voltage ? (As per TI app note slyt777.pdf )
I assumed will work for both LDO and BUCK ??
Can you please share your feedback.
Thanks and Regards,
Arumugam.P
Hello Arugarum,
I am part of the Low Voltage input (<7V Vin) Buck team and your query for the LDO will be handled by a member of the Applications team from the LDO team.
Would you be then interested in looking into the QFN version of the TPS62864 ?
As this is material soon to be released we could continue this discussion via email.
Let me know if you need help for your TPS62823 design!
Thanks a lot!
Regards,
Dorian
Dear Dorian,
Thanks for your support.
Yes we can start through email .
My product is going to be go for manufacturing with in 4 to 6 weeks.
When the QFN package is available for user ?
Thanks and Regards,
Arumugam.P
Hello Arumugam,
Can you accept my friendship request so we can talk via private message ?
Thanks a lot!
Regards,
Dorian
Hello Arumugam,
I sent you a private message.
In the meantime, I will close this thread here as we are discussing on a private thread.
Thanks a lot!
Regards,
Dorian
Dear Dorian,
Thanks for your support.
Also volumes we may not able to confirm considering current phase of project.
If need any more details please let me know.
I need you support to review the schematics for PMIC card which includes BUCK , LDO and DAC.
Can I send the schematics for review through email.
Not delivering your private email.
you can send email to arumugamp@eximiusdesign.com