Hi,6204.BQ25713_Ckt.pdfbq25713_i2c_write and read info updated .xlsx
We are using BQ25713 as part of Battery Management System.
The schematic implementation is captured herewith. The only change in schematic is C44 - we have replaced 1uF cap with 2.2uF cap.
We have set it for 3S battery configuration to get about 10V or above output.
Please find the attached register setting that we have carried out when we have both battery and main connected.
The system works fine with Vsys having desired level when we have battery only present.
The system also works fine when we have both battery and adapter input present and we get desired Vsys.
But when we just have Vsys connected and no battery connected, we do not get Vsys. Vsys voltage drops to almost <1V when only main is present and no battery.
This means we can not even write into registers as Vsys is the one that is used to get all other voltages like 3.3v / 5v for further usage.
Any idea why Vsys does not come when we have just adapter supply available and no battery connected?
Are there any connectivity that we need to change or modify in schematic to enable this adapter to Vsys supply availability?
Thanks and warm regards
Dharin