Hi Team,
My customer is using TPS26602 and have 2 questions.
1.Overload response time
Customer is using Active current limiting mode, want to make sure it can pass a ms-time overload caused by Hotswap, and need our test data.
Refer to datasheet,
In Electronic circuit breaker mode, when the I(load)>I(CB) longer than 4ms, the device turns OFF the internal FET and FLT is asserted.
In Active current limiting mode, the internal FET is turn off until the device junction temperature reaches the thermal shutdown threshold (T(TSD)).
Is the time to reach the shutdown threshold in Active current limiting mode much longer than 4ms t(CB)_delay in Electronic circuit breaker mode or not?
Do we have related test result show specific response time in active limiting mode?
2.OVP Pin connection.
Refer to the datasheet, TPS26602 OVP pin must connect to RTN directly, but they connected as resistor divider like TPS26600 application circuit in datasheet. However, it turns out that TPS26602 can clamp at 38V in input overvoltage.
Is it OK to connect resistor between OVP and RTN pin for TPS26602? Is there any potential risk to do as this?
Thank you!
Yunjing