Hi,
I want BQ25703A to disable supply from battery when I am shutting down my processor.
Is there a way to use I2C to control Batdrv output? If yes, what are the registers to use?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want BQ25703A to disable supply from battery when I am shutting down my processor.
Is there a way to use I2C to control Batdrv output? If yes, what are the registers to use?
Thank you
Hi John,
You can put the converter into HIz mode (either pull pin 6 ILIM_HIZ to ground, or set REG0x35[7] to 1) and then while in HIz mode, turn off the BATFET (REG34[1] to 1).